Write-only
About Source Power Calibration

ApplySourcePowerCalibrationTo Method


Description

Copies and applies an existing Source Power Calibration to another channel.

 VB Syntax

chan.ApplySourcePowerCalibrationTo (fromPortNum, targetChan, targetPortNum);

Variable

(Type) - Description

chan

A Channel (object)

fromPortNum

(Long) Port number of the existing source power correction.

targetChan

(Long) Channel number to which the source power correction will be copied.

targetPortNum

(Long) Port number to which the source power correction will be applied.

Return Type

Not Applicable

Default

Not Applicable

Examples

chan.ApplySourcePowerCalibrationTo 1,2,1

C++ Syntax

HRESULT ApplySourcePowerCalibrationTo (long fromPortNumber, long otherChannelNumber, long portNumber);

Interface

IChannel11