Channel Object


See SourcePowerCalData Interface for putting and getting typed source power calibration data.

Description

The channel object is like the engine that produces data. Channel settings consist of stimulus values like frequency, power, IF bandwidth, and number of points.

Accessing the Channel object

You can get a handle to a channel in a number of ways. But first you have to make sure that the channel exists. When you first startup the analyzer, there is one S11 measurement on channel 1. Thus there is only one channel in existence. You can do the following:

Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)

Dim chan As IChannel
Set chan = app.ActiveChannel

or

Set chan = app.Channels(2)

The first method returns the channel object that is driving the active measurement.  If there is no measurement, there may not be a channel. Once a channel is created, it does not go away. So if there once was a measurement (hence a channel), the channel will still be available.

If there is no channel you can create one in a couple ways. You can do the following:

Pna.CreateMeasurement( ch1, "S11", port1, window2)

or

Pna.Channels.Add(2)

The latter will have no visible effect on the analyzer. It will simply create channel 2 if it does not already exist.

See Also:

(Bold Methods or Properties provide access to a child object)

Methods

Interface

See History

Description

Abort

IChannel

Aborts the current measurement sweep on the channel.

ApplySourcePowerCorrectionTo

IChannel11

Copies an existing Source Power Calibration to another channel.

AveragingRestart

IChannel

Clears and restarts averaging of the measurement data.

Continuous

IChannel

The channel continuously responds to trigger signals.

CopyToChannel

IChannel2

Sets up another channel as a copy of this objects channel.

FrequencySpanFull

IChannel25

Sets the frequency span to the entire frequency range of the analyzer.

GetConverter

IChannel17

Returns a handle to a Converter object.

GetErrorCorrection

IChannel8

Returns the channel error correction state.

GetNumberOfGroups

IChannel4

Returns the number of groups a channel has yet to acquire.

GetPortNumber

IChannel13

Returns the port number for the specified string port name.

GetRxLevelingConfiguration

IChannel17

Returns a handle to a RxLevelingConfiguration object

getSourcePowerCalData

IChannel

Superseded with Get SourcePowerCalDataEx

getSourcePowerCalDataEx

IChannel4

Returns requested source power calibration data, if it exists.

GetSupportedALCModes

IChannel10

Returns a list of supported ALC modes

GetXAxisValues

IChannel

Returns the channel's X-axis values into a dimensioned Variant array.

GetXAxisValues2

IChannel

Returns the channel's X-axis values into a dimensioned NON-Variant array.

Hold

IChannel

Puts the Channel in Hold - not sweeping.

Next_IFBandwidth

IChannel

A function that returns the Next higher IF Bandwidth value.

NumberOfGroups

IChannel

Sets the Number of trigger signals the channel will receive.

Preset

IChannel

Resets the channel to factory defined settings.

PreviousIFBandwidth

IChannel

Returns the previous IF Bandwidth value.

putSourcePowerCalData

IChannel

Superseded with Put SourcePowerCalDataEx Method

putSourcePowerCalDataEx

IChannel4

Inputs source power calibration data to this channel for a specific source port.

SelectCalSet

IChannel

Specifies the Cal Set to use for the Channel

Single

IChannel

Channel responds to one trigger signal from any source (internal, external, or manual). Then channel switches to Hold.

UnselectCalset

IChannel24

Unselects a Cal Set from the specified channel.

Properties

Interface

Description

ALCLevelingMode

IChannel10

Set or return the ALC leveling mode.

AlternateSweep

IChannel

Sets sweeps to either alternate or chopped.

Attenuator

IChannel

Sets or returns the value of the attenuator control for the specified port number.

AttenuatorMode

IChannel

Sets or returns the mode of operation of the attenuator control for the specified port number.

AuxiliaryTrigger

IChannel10

Provides access to  Auxiliary Triggering

Averaging

IChannel

Turns trace averaging ON or OFF for all measurements on the channel.

AveragingCount

IChannel

Returns the number of sweeps that have been averaged into the measurements.

AveragingFactor

IChannel

Specifies the number of measurement sweeps to combine for an average.

AverageMode

IChannel16

Sets Point or Sweep averaging.

BalancedTopology

IChannel6

Provides access to  the topology of a balanced DUT.

Calibrator

IChannel4

Provides access to Unguided calibration.

CalSet

IChannel7

Provides access to the contents of a Cal Set

centerFrequency

IChannel

Sets or returns the center frequency of the channel.

Shared with the Segment Object

CenterFrequencyStepSize

IChannel25

Sets and reads the center frequency step size of the analyzer.

CenterFrequencyStepSizeMode

IChannel25

Sets and reads how the center frequency step size is determined.

channelNumber

IChannel

Returns the Channel number.

Shared with the Measurement Object

Converter

IChannel21

Provides access to a mixer/converter object.

CorrectionMethods

IChannel21

Provides access to channel correction properties.

CoupleChannelParams

IChannel5

Turns ON and OFF Time Domain Trace Coupling.

CouplePorts

IChannel

Turns ON and OFF port power coupling.

CustomChannelConfiguration

IChannel12

Provides access to custom application objects.

CWFrequency

IChannel

Set the Continuous Wave (CW) frequency.

DCStimulus

IChannel23

Provides access to the DCStimulus object.

DefinedRoles

IChannel22

Returns the roles for which sources can be used for the channel.

DwellTime

IChannel

Sets or returns the dwell time for the channel.

Shared with the Segment Object

ErrorCorrection

IChannel7

Attempts to sets error correction ON or OFF for all of the measurements on the channel.

ExternalTriggerDelay

IChannel6

Sets or returns the external trigger delay value for the channel.

FastCWPointCount

IChannel16

Enables Fast CW sweep and sets the number of data points for the channel.

Fixturing

IChannel6

Provides access to Port Ext, Embedding, and De-embedding functions.

FOM Collection

IChannel9

Provides access to Frequency Offset Measurements

FrequencyOffsetDivisor

IChannel2

 

FrequencyOffsetFrequency

IChannel2

 

FrequencyOffsetMultiplier

IChannel2

Superseded with FOM and FOMRange

FrequencyOffsetCWOverride

IChannel2

 

FrequencyOffsetState

IChannel2

 

FrequencySpan

IChannel

Sets or returns the frequency span of the channel.

Shared with the Segment Object.

FrequencyStep

IChannel24

Sets the frequency step size across the selected frequency range.

IFBandwidth

IChannel

Sets or returns the IF Bandwidth of the channel.

Shared with the Segment Object.

IFConfiguration

IChannel4

Provides access to the IF gain and source path settings for the H11 Option.

IsBlocked

IChannel19

Returns whether or not a channel is blocked from sweeping.

IsContinuous

IChannel4

Returns whether or not a channel is in continuous mode.

IsHold

IChannel4

Returns whether or not a channel is in hold mode.

LowFrequencyExtension

IChannel26

Enables low frequency extension (LFE).

MeasurementClass

IChannel15

Returns the measurement class name.

MultiDimensionalSweep

IChannel27

Provides access to the MultiDimensionalSweep Object.

NumberOfPoints

IChannel

Sets or returns the Number of Points of the channel.

Shared with the Segment Object.

Parent

IChannel

Returns a handle to the parent object of the channel.

PathConfiguration

IChannel10

Provides access to path configuration switches and setting.

PathConfigurationManager

IChannel10

Provides access to path configuration file management.

PhaseControl

IChannel21

Provides access to the PhaseControl object.

PointSweepState

IChannel16

Turns point sweep ON or OFF for all measurements on the channel.

PowerSlope

IChannel

Sets or returns the Power Slope value.

PowerSlopeState

IChannel18

Turns power slope ON or OFF

PulseGenerator

IChannel10

Provides access to pulse generator configuration.

PulseGeneratorID

IChannel23

Returns the ID for the specified Pulse Generator name.

PulseGeneratorNames

IChannel23

Returns a list of configured Pulse Generator names.

PulseMeasControl

IChannel20

Provides access to pulse measurement settings.

R1InputPath

IChannel2

Throws internal reference switch.

ReceiverAttenuator

IChannel

Sets or returns the value of the specified receiver attenuator control.

ReduceIFBandwidth

IChannel5

Sets or returns the state of the Reduced IF Bandwidth at Low Frequencies setting.

RoleDevice

IChannel22

Sets and returns the source to be used in the specified role.

RXLevelingConfiguration

IChannel21

Provides access to the ReceiverLeveling Object

Segments

IChannel

Provides access to the Collection for iterating through the sweep segments of a channel.

SignalProcessingModuleFour

IChannel10

Provides access to the SignalProcessingModuleFour object.

SourcePortCount

IChannel13

Returns the number of source ports.

SourcePortFixedFrequency

IChannel27

Set and read the fixed frequency value for a specific port.

SourcePortMode

IChannel9

Sets the state of the VNA sources. (AUTO | ON | OFF)

SourcePortNames

IChannel13

Returns the string names of source ports.

SourcePortStartFrequency

IChannel27

Set and read the start frequency value for a specific port.

SourcePortStopFrequency

IChannel27

Set and read the stop frequency value for a specific port.

SourcePowerCalPowerOffset

IChannel4

Sets or returns a power level offset from the VNA test port power.

SourcePowerCorrection

IChannel

Turns source power correction ON or OFF for a specific source port.

StartFrequency

IChannel

Sets or returns the start frequency of the channel.

Shared with the Segment Object

StartPower

IChannel

Sets the start power of the analyzer when sweep type is set to Power Sweep.

StartPowerEx

IChannel13

Sets and reads the power sweep start power value for a specific port.

StopFrequency

IChannel

Sets or returns the stop frequency of the channel.

Shared with the Segment Object

StopPower

IChannel

Sets the Stop Power of the analyzer when sweep type is set to Power Sweep.

StopPowerEx

IChannel13

Sets and reads the power sweep stop power value for a specific port.

SweepDelay

IChannel19

Sets the time to wait just before acquisition begins for each sweep.

SweepGenerationMode

IChannel

Sets the method used to generate a sweep: continuous ramp (analog) or discrete steps (stepped).

SweepSpeedMode

IChannel14

Set or returns the sweep speed mode.

SweepTime

IChannel

Sets the Sweep time of the analyzer.

SweepType

IChannel

Sets the type of X-axis sweep that is performed on a channel.

TestPortPower

IChannel

Sets or returns the RF power level for the channel.

Shared with the Segment Object

TriggerMode

IChannel

Determines the measurement that occurs when a trigger signal is sent to the channel.

UserRangeMax

IChannel

Superseded - Use meas.UserRangeMax

Sets the stimulus stop value for the specified User Range.

UserRangeMin

IChannel

Superseded - Use meas.UserRangeMin

Sets the stimulus start value for the specified User Range.

XAxisPointSpacing

IChannel

Sets X-Axis point spacing for the active channel.

IChannel History

Interface

Introduced with VNA Rev:

IChannel

1.0

IChannel2

3.0

IChannel3

4.0

IChannel4

4.0

IChannel5

4.2

IChannel6

5.0

IChannel7

5.2

IChannel8

6.0

IChannel9

7.0

IChannel10

7.2

IChannel11

7.5

IChannel12

8.0

IChannel13

8.2

IChannel14

8.33

IChannel15

8.33

IChannel16

8.35

IChannel17

8.55

IChannel19

9.20

IChannel20

9.20

IChannel21

9.30

IChannel22

9.42

IChannel23

9.50

IChannel24

10.40

IChannel25

10.45

IChannel26

12.80

IChannel27

13.25

ISourcePowerCalData Interface


Description

Contains methods for putting source power calibration data in and getting source power calibration data out of the analyzer using typed data.  The methods in this interface transfer data more efficiently than methods that use variant data. However, this interfaces is only usable from VB6, C, & C++.  All other programming languages must use the methods on the Channel Object.

Note: Interface ISourcePowerCalData is abbreviated as ISPCD in the following table.

 

Methods

Interface

See History

Description

getSourcePowerCalDataScalar

ISPCD

Superseded  - use PutSourcePowerCalDataScalarEx Method

getSourcePowerCalDataScalarEx

ISPCD2

Returns requested source power calibration data, if it exists.

putSourcePowerCalDataScalar

ISPCD

Superseded  - use PutSourcePowerCalDataEx Method

putSourcePowerCalDataScalarEx

ISPCD2

Inputs source power calibration data to a channel, for a specific source port.

Properties

 

Description

None

 

 

 

ISourcePowerCalData History

Interface

Introduced with VNA Rev:

ISourcePowerCalData

2.0

ISourcePowerCalData2

4.0