Write-only
About Auto Port Extensions

AutoPortExtMeasure Method


Description

Measures either an OPEN or SHORT standard. When this command is sent, the VNA acquires the measurement with which to set automatic port extensions. Learn more about choosing which standard to measure.

 VB Syntax

fixture.AutoPortExtMeasure value

Variable

(Type) - Description

fixture

A Fixturing (object)

value

(Enum as NAAutoPortExtMeasure)

0 - naAPEM_OPEN - Measure OPEN

1 - naAPEM_SHORT - Measure SHORT

Return Type

ENUM

Default

Not Applicable

Examples

fixture.AutoPortExtMeasure naAPEM_OPEN

C++ Syntax

HRESULT get_AutoPortExtMeasure(tagNAAutoPortExtMeasure *pVal );

Interface

IFixturing2