Fixturing Object


Description

Contains the properties for Embedding and De-embedding test fixtures.

Accessing the Fixturing object

Dim app as AgilentPNA835x.Application
Dim chan as Channel
Set chan = app.ActiveChannel
Dim fixt as Fixturing
Set fixt = chan.Fixturing

See Also:

Methods

 

Description

AutoPortExtMeasure

IFixturing2

Measures either an OPEN or SHORT standard.

AutoPortExtReset

IFixturing2

Clears old port extension delay and loss data.

NetworkPortMap

IFixturing2

Set the port mapping for a 4-port SNP file to be embedded.

Properties

Interface

See History

Description

AutoPortExtConfig

IFixturing2

Sets the frequency span that is used to calculate Automatic Port Extension.

AutoPortExtDCOffset

IFixturing2

Specifies whether or not to include DC Offset as part of Automatic port extension.

AutoPortExtLoss

IFixturing2

Specifies whether or not to include loss correction as part of Automatic Port Extension.

AutoPortExtSearchStart

IFixturing2

Set the start frequency for custom user span.

AutoPortExtSearchStop

IFixturing2

Set the stop frequency for custom user span.

AutoPortExtState

IFixturing2

Enables and disables automatic port extensions on the specified port.

CmnModeZConvPortImag

IFixturing2

Sets imaginary value for common port impedance conversion.

CmnModeZConvPortReal

IFixturing2

Sets real value for common port impedance conversion.

CmnModeZConvState

IFixturing2

Turns ON/OFF common port impedance conversion.

CmnModeZConvPortZ0

IFixturing2

Sets impedance value for common port impedance conversion.

DiffPortMatch_C

IFixturing2

Sets Capacitance value of the differential matching circuit.

DiffPortMatch_G

IFixturing2

Sets Conductance value of the differential matching circuit.

DiffPortMatch_L

IFixturing2

Sets Inductance value of the differential matching circuit.

DiffPortMatch_R

IFixturing2

Sets Resistance value of the differential matching circuit.

DiffPortMatchMode

IFixturing2

Sets type of circuit to embed.

DiffPortMatchUserFilename

IFixturing2

Specifies the 4-port touchstone file for user-defined differential matching circuit.

DiffPortMatchState

IFixturing2

Turns ON/OFF differential matching circuit function.

DiffZConvPortImag

IFixturing2

Sets imaginary value for differential port impedance conversion.

DiffZConvPortReal

IFixturing2

Sets real value for differential port impedance conversion.

DiffZConvPortZ0

IFixturing2

Sets impedance value for differential port impedance conversion.

DiffZConvState

IFixturing2

Turns ON/OFF differential port impedance conversion.

Embed4PortA

IFixturing2

Returns VNA portA connections.

Embed4PortB

IFixturing2

Returns VNA portB connections.

Embed4PortC

IFixturing2

Returns VNA portC connections.

Embed4PortD

IFixturing2

Returns VNA portD connections.

Embed4PortList

IFixturing2

Specifies all VNA port connections.

Embed4PortNetworkFilename

IFixturing2

Specifies *.s4p filename.

Embed4PortNetworkMode

IFixturing2

Specify embed, de-embed, or none.

Embed4PortState

IFixturing2

Turns ON or OFF 4-port Network Embed/De-embed.

Embed4PortTopology

IFixturing2

Specifies the VNA / DUT topology.

EnablePowerCompensation

IFixturing5

Compensates source power for combined loss through all fixturing functions.

EnableSnPDataExtrapolation

IFixturing6

Turns ON and OFF SNP file extrapolation for both 2-port and 4-port embedding/de-embedding.

FixturingState

IFixturing

Turns Fixturing ON and OFF on this channel.

NetworkPortMapA

IFixturing6

Read the port mapping of in A port for a 4-port SNP file to be embedded.

NetworkPortMapB

IFixturing6

Read the port mapping of in B port for a 4-port SNP file to be embedded.

NetworkPortMapC

IFixturing6

Read the port mapping of out A port for a 4-port SNP file to be embedded.

NetworkPortMapD

IFixturing6

Read the port mapping of out B port for a 4-port SNP file to be embedded.

Port2PdeembedCktModel

IFixturing

Sets and returns the 2 port De-embedding circuit model for the specified port number.

Port2PdeembedState

IFixturing

Turns 2 port de-embedding ON and OFF on this channel.

PortArbzImag

IFixturing3

Sets and returns the imaginary impedance value for the specified single-ended port number.

PortArbzReal

IFixturing3

Sets and returns the real impedance value for the specified single-ended port number.

PortArbzState

IFixturing

Turns single-ended port impedance ON and OFF on the specified channel.

PortArbzZ0

IFixturing3

Sets and returns the real and imaginary impedance value for the specified single-ended port number.

PortCoupleToSystemMedia

IFixturing4

Couples to system Media type

PortCoupleToSystemVelocity

IFixturing4

Couples to system Velocity Factor

PortDelay

IFixturing

Sets and returns the Port Delay value for the specified port number.

PortDistance

IFixturing4

Sets Port Ext in distance

PortNADistanceUnit

IFixturing4

Sets distance units

PortExtState

IFixturing

Turns Port Extension ON and OFF on this channel.

PortExtUse1

IFixturing

Sets and returns the USE1 ON/OFF state for the Loss1 and Freq1 values for the specified port number.

PortExtUse2

IFixturing

Sets and returns the USE2 ON/OFF state for the Loss2 and Freq2 values for the specified port number.

PortFreq1

IFixturing

Sets and returns the 1st Port Frequency value for the specified port number.

PortFreq2

IFixturing

Sets and returns the 2nd Port Frequency value for the specified port number.

PortLoss1

IFixturing

Sets and returns the 1st Port Loss value for the specified port number.

PortLoss2

IFixturing

Sets and returns the 2nd Port Loss value for the specified port number.

PortLossDC

IFixturing

Sets and returns the Port Loss at DC value for the specified port number.

PortMatching_C

IFixturing7

Sets and returns the Capacitance, 'C' value for the specified port number.

PortMatching_G

IFixturing7

Sets and returns the Conductance, 'G' value for the specified port number.

PortMatching_L

IFixturing7

Sets and returns the Inductance, 'L' value for the specified port number.

PortMatching_R

IFixturing7

Sets and returns the Resistance, 'R' value for the specified port number.

PortMatchingCktModel

IFixturing

Sets and returns the Port Matching circuit model for the specified port number.

PortMatchingState

IFixturing

Turns Port Matching ON and OFF on this channel.

PortMedium

IFixturing4

Sets Media per port

PortVelocityFactor

IFixturing4

Set Velocity Factor per port

PortWGCutoffFreq

IFixturing4

Sets waveguide cutoff frequency per port

Reverse2PortAdapter

IFixturing6

Set and read whether or not to reverse ports on a 2-port fixture or adapter to be de-embedded.

strPort2Pdeembed_S2PFile

IFixturing

Sets and returns the 2 port De-embedding 'S2P' file name for the specified port number.

strPortMatch_S2PFile

IFixturing

Sets and returns the Port Matching 'S2P' file name for the specified port number.

IFixturing History

Interface

Introduced with VNA Rev:

IFixturing

5.0

IFixturing2

5.2

IFixturing3

5.25

IFixturing4

8.50

IFixturing5

9.20

IFixturing6

9.33

IFixturing7

12.70