Description |
This command is replaced with CreateCustomMeasurementEx Method. Creates a new custom measurement. |
VB Syntax |
app.CreateCustomMeasurement chanNum,guid[,window] |
Variable |
(Type) - Description |
app |
(object) - An Application object |
chanNum |
(long) -Channel number used by the new measurement; can exist or be a new channel. |
guid |
(string) - the GUID (Globally Unique IDentifier) of the new custom measurement object. The new custom measurement must be installed and registered on the PNA. Should be in “registry format”. See example below. |
window |
(long) Optional argument. Number of the window the new custom measurement will be placed in. Choose 1 to 16. If unspecified, the measurement is placed in the active window. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.CreateCustomMeasurement 1, "{12345678-56D3-11D5-AD50-00108334AE98}" 'Not an actual custom measurement - for example purpose only |
C++ Syntax |
HRESULT CreateCustomMeasurement (long ChannelNum, BSTR guid, long windowNumber) |
Interface |
IApplication |