Meas
Class |
Measurement Name |
Description |
"Standard" |
"S11",
"S21", and
so forth
"A_1","A_2",
and so forth |
S-parameter
name
Unratioed parameter names with notation: "receiver_source
port"
See Balanced
S-parameter measurement names |
Active Hot Parameters |
"HotS11"
"HotS31"
"HotS13"
"HotS33"
"IPwr"
"OPwr"
"Gamma"
"Pmax"
"Xs(3,3)"
"Xt(3,3)"
"Xf(3,1)"
"DeltaOPwr" |
Learn
about Active Hot parameters |
"Vector
Mixer/Converter" |
"S11"
"VC21"
"S22" |
Learn
about VMC parameters |
"Scalar
Mixer/Converter" |
"S11"
"SC21"
"SC12"
"S22"
"Ipwr"
"RevIPwr"
"Opwr"
"RevOPwr" |
Learn
about SMC parameters |
"Gain
Compression"
Learn
more
"Gain
Compression Converters"
Learn
more |
GCA
and GCX: |
"CompIn21" |
Input
power at the compression point. |
"CompOut21" |
Output
power at the compression point. |
"CompGain21" |
Gain at
the compression point. |
"CompS11" |
Input
Match at the compression point |
"RefS21" |
Linear
Gain |
"DeltaGain21" |
CompGain21
-Linear Gain |
"S11",
"S21", "S12", "S22" |
Standard
S-parameters; measured at port 1 and port 2 |
GCX
- All Gain Compression
parameters (except S21 and S12) plus the following: |
"S11"
"SC21"
"SC12"
"S22"
"Ipwr"
"RevIPwr"
"Opwr"
"RevOPwr" |
Mixer parameters |
"Modulation Distortion"
Learn
more |
Modulation Distortion: |
"POut2" |
Power
Out |
"PIn1" |
Power
In |
"MSig2" |
Modulation
Signal Out |
"MDist2" |
Modulation
Distortion Out |
"MGain21" |
Modulation
Gain |
"MComp21" |
Modulation Compression |
"PGain21" |
Power Gain |
"S11" |
Linear Input Match |
"S21" |
Linear Gain |
"LPIn1" |
Linear Input Match |
"LPOut1" |
Linear Reflected Power In |
"LPOut2" |
Linear Power Out |
"A",
"b1" |
Port 1 test port receiver |
"B",
"b2" |
Port 2 test port receiver |
"R1",
"a1" |
Port 1 reference receiver |
"R2",
"a2" |
Port 2 reference receiver |
"CarrIn1" |
Input Band Power |
"CarrOut2" |
Output Band Power |
"CarrGain21" |
Band Power Gain |
"ACPIn1" |
ACP at input |
"ACPOut2" |
ACP at output |
"ACPDist21" |
ACP distortion, Added by DUT |
"EVMDistEq21" |
EVM Equalized Distortion,
Added by DUT |
"EVMDistUn21" |
EVM Unequalized Distortion,
Added by DUT |
"Noise
Figure Cold Source"
Learn
more
"Noise Figure Converters"
Learn
more |
Noise
Figure AND NFX: |
"NF" |
Noise figure |
"ENR" |
Validate noise source
measurements. |
"T-Eff" |
Effective noise temperature. |
"DUTRNP"
"DUTRNPI" |
DUT noise power ratio.
(Noise power expressed in Kelvin divided by 290). |
"SYSRNP"
"SYSRNPI" |
System noise power ratio |
"DUTNPD"
"DUTNPDI" |
DUT noise power density.
(Noise power expressed in dBm/Hz). |
"SYSNPD"
"SYSNPDI" |
System noise power density.
|
"OvrRng"
(Opt 029 Only) |
Indication that the noise
receiver is being over powered. |
"T-Rcvr"
(Opt
029 Only) |
Temperature reading (in
Kelvin) of the noise receiver board. |
Noise
Figure ONLY - NOT NFX: |
"S11",
"S21", "S12", "S22" |
Standard S-parameters;
measured with the port1 and port2 noise switches set for
noise mode. |
"A_1","A_2"
...and so forth. |
Unratioed
parameters; with notation:
"receiver, source port" |
"GammaOpt" |
Optimum
Complex Reflection Coefficient |
"Rn" |
Noise
Resistance |
"NFMin" |
Minimum noise figure that
occurs at GammaOpt |
NFX
ONLY: |
"S11"
"SC21"
"SC12"
"S22"
"Ipwr"
"RevIPwr"
"Opwr"
"RevOPwr" |
Mixer parameters |
"ALO1","
BLO1" ...and so
forth. |
Test port receiver at
LO1 frequency |
"R1_1",
"B_2" ..and
so forth. |
Unratioed parameters with
notation:
"receiver_source port" |
Phase Noise
Learn
more |
|
|
PN |
Phase Noise |
AM |
AM Noise |
"Swept IMD"
"Swept IMD Converters"
Learn
more |
There
are over 150 possible Swept IMD parameters, too many to
list here.
Build the parameters with
the Swept
IMD Parameter dialog, then copy the parameter name
to the remote command.
The following are a few
example parameters: |
"PwrMainLo" |
Absolute power of the
Low tone at the DUT output. |
"IM3" |
Power of the third product
relative to the average power of the f1 and f2 tones measured
at the DUT output. |
"OIP3" |
Theoretical power level
at which the third product will be the same power level
as the average of the main tones at the output of the
DUT. |
"IM Spectrum"
Learn
more |
"Output" |
View signals OUT of the
DUT and into VNA port 2 (B receiver). |
"Input" |
View signals IN to the
DUT (R1 receiver). |
"Reflection" |
View signals reflected
off the DUT input and back into VNA port 1 (A receiver) |
"IMx
Spectrum Converters"
Learn
more |
"Output" |
View signals OUT of the
DUT and into VNA port 2 (B receiver) |
"Differential
I/Q"
Learn
more |
Create custom parameters
using DefineParameter
Method, then specify your custom parameter name here.
The following are default parameters: |
"IPwrF1"
"OPwrF1"
"GainF1" |
Input Power over F1 range
Output Power over F1 range
Gain over F1 range |
"Spectrum
Analyzer"
Learn
more |
"a<n>"
"b<n>"
where
<n> is the
port number to measure
"ImageReject<n>"
where
<n> is the image reject trace |
Reference
receiver
Test port receiver |