Write-only
About Mixer/Converter Settings

DeleteAllSegments Method


Description

Removes all segments from the scratch mixer.

 VB Syntax

conv.DeleteAllSegments( )

Variable

(Type) - Description

conv

A Converter Object

Return Type

Not Applicable

Default

Not Applicable

Examples

mxr.DeleteAllSegments()

See example program

C++ Syntax

HRESULT DeleteAllSegments()

Interface

IConverter5