Write-only
About Mixer/Converter Settings

DeleteSegment Method


Description

Removes the specified number of segments from the scratch mixer starting at the index position.

 VB Syntax

conv.DeleteSegment index,count

Variable

(Type) - Description

conv

A Converter Object

index

(Long integer) Position at which to start removing segments. Valid index range is between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer.

count

(Long integer) Optional argument. Number of segments to remove. If unspecified, 1 segment is removed.

Return Type

Not Applicable

Default

Not Applicable

Examples

mxr.DeleteSegment 1,5 'Removes 5 segments beginning at the first position.

See example program

C++ Syntax

HRESULT DeleteSegment(long index, long count);

Interface

IConverter5