Description |
Returns an array of max leveled power values (in dBm), where each element corresponds to the maximum leveled power possible for CW stimulus at the corresponding frequency set by the DiscreteFrequencies property. |
VB Syntax |
maxPower = powerRange.DiscreteGetMaxPowerArray |
Variable |
(Type) - Description |
powerRange |
A PowerRange (object) |
maxPower |
(Variant array) Variable to store the list of maximum leveled power values in dBm. |
Return Type |
Variant array |
Default |
Not Applicable |
maxPower = powerRange.DiscreteGetMaxPowerArray |
|
C++ Syntax |
HRESULT get_DiscreteGetMaxPowerArray(VARIANT* pMax); |
Interface |
IPowreRange |