Write / Read
About Receiver Leveling

DiscreteFrequencies Property


Description

Sets or returns the list of discrete frequencies corresponding to the powers returned by DiscreteGetMaxPowerArray or DiscreteGetMinPowerArray.

 VB Syntax

powerRange.DiscreteFrequencies = discreteFreqs

Variable

(Type) - Description

powerRange

A PowerRange (object)

discreteFreqs

(Variant array) Variable to store the list of discrete frequencies.

Return Type

Variant array

Default

Not Applicable

 

discreteFreqs = Array(1e9,2e9,3e9,4e9) 'Write
powerRange.DiscreteFrequencies = discreteFreqs 'Read

C++ Syntax

HRESULT get_DiscreteFrequencies(VARIANT* Freq);

HRESULT put_DiscreteFrequencies(VARIANT Freq);

Interface

IPowreRange