Read only |
About VNA Options |
Description |
Returns the port number that is associated with the specified port name. These numbers are used with several commands to specify a VNA port. To learn more, see Remotely Specifying a Source Port. |
VB Syntax |
value = object.GetPortNumber (portName) |
Variable |
(Type) - Description |
|
value |
(Long) - Variable to store the returned Port Number integer value. |
|
object |
A Channel (object) - always more complete than capabilities object. A Capabilities (object) - use when a channel is not available |
|
portName |
(String) Name of the VNA port.
|
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
value = chan.GetPortNumber ("Src2 Out1") 'Read |
C++ Syntax |
HRESULT GetPortNumber(BSTR name, long *number); |
Interface |
IChannel13 ICapabilities4 |