Read-only

GetECALModuleInfoEx Method


Description

This property replaces Get ECALModuleInfo Method.

Returns the following information about the connected ECAL module: model number, serial number, connector type, calibration date, min and max frequency.

The characterization within the ECal module that this information will be read from is specified by ECALCharacterizationEx.  The default value is 0.

 VB Syntax

moduleInfo = cal.GetECALModuleInfoEx (module)

Variable

(Type) - Description

moduleInfo

(string) - variable to store the module information

cal

A Calibrator (object)

module

(long integer)  ECal module.

Choose from modules 1 through 8

Use IsECALModuleFoundEx to determine the number of modules connected to the VNA

Return Type

String

Default

Not Applicable

Examples

info = cal.GetECALModuleInfoEx(2)

Example return string:

ModelNumber: 85092-60007, SerialNumber: 01386, ConnectorType: N5FN5F, PortAConnector: Type N (50) female, PortBConnector: Type N (50) female, MinFreq: 30000, MaxFreq: 9100000000, NumberOfPoints: 250, Calibrated: July 4 2002

C++ Syntax

HRESULT GetECALModuleInfoEx(long moduleNumber, BSTR* info);

Interface

ICalibrator4