Read-only

GetECALModuleInfo Method - Superseded


Description

Note: This property is replaced by GetECALModuleInfoEx Method

Returns the following information about the connected ECAL module: model number, serial number, connector type, calibration date, min and max frequency.

The characterization within the ECal module that this information will be read from is specified by the ECALCharacterization property on the ICalibrator2 interface.  The default value of the ECALCharacterization property is naECALFactoryCharacterization.

 VB Syntax

moduleInfo = cal.GetECALModuleInfo (module)

Variable

(Type) - Description

moduleInfo

(string) - variable to store the module information

cal

A Calibrator (object)

module

(enum NAECALModule) – ECAL module. Choose from:

0 - naECALModule_A

1 - naECALModule_B

Return Type

String

Default

Not Applicable

Examples

info = cal.GetECALModuleInfo(naECALModule_A)

Example return string:

ModelNumber: 85092-60007, SerialNumber: 01386, ConnectorType: N5FN5F, PortAConnector: Type N (50) female, PortBConnector: Type N (50) female, MinFreq: 30000, MaxFreq: 9100000000, NumberOfPoints: 250, Calibrated: July 4 2002

C++ Syntax

HRESULT GetECALModuleInfo(tagNAECALModule ecalModule, BSTR* info);

Interface

ICalibrator