Write-only
About Triggering

Hold (channels) Method


Description

Places ALL channels in hold mode.

To resume all channels sweeping, use chans.Resume. (Must be the same instance of chans).

To place a single channel in hold mode, use channel.Hold Method.

VB Syntax

chans.Hold

Variable

(Type) - Description

chans

A Channel collection (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

chans.Hold

C++ Syntax

HRESULT Hold();

Interface

IChannels2