Write-only
About Triggering

Resume Method


Description

Resumes the trigger mode of all channels that was in effect before sending  the channels.Hold method. Channels.Hold must be sent before channels.Resume, using the same instance of the Channels object.

VB Syntax

chans.Resume

Variable

(Type) - Description

chans

A Channel collection (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

chans.Resume

C++ Syntax

HRESULT Resume();

Interface

IChannels2