Read-only
About Independent Power Calibration

Item (Independent Power Calibration Port) Method


Description

This method returns a handle to the IndependentPowerCalibrationPort object.

 VB Syntax

IndependentPwrrCal.Item

Variable

(Type) - Description

IndependentPwrrCal

A IndependentPowerCalibration (object)

Return Type

IIndependentPowerCalibrationPort

Default

Not Applicable

Example

CalibrateAllChannels.IndependentPowerCalibration.Item

C++ Syntax

HRESULT Item( IIndependentPowerCalibrationPort** value);

Interface

IIndependentPowerCalibration