Write-only
About 4-Port Fixturing

NetworkPortMap Method


Description

Set the port mapping for a 4-port SNP file to be embedded.

To read port mapping, use NetworkPortMapA, NetworkPortMapB, NetworkPortMapC, NetworkPortMapD.

 VB Syntax

fixture.NetworkPortMap network, inA, inB, outA, outB

Variable

(Type) - Description

fixture

A Fixturing (object)

network

Network position. Choose from 1 or 2.

inA, inB, outA, outB

Port Mapping. Use four port numbers in any order.

Return Type

Not Applicable.

Default

1,2,3,4

Examples

fixture.NetworkPortMap 1,1,3,2,4

C++ Syntax

HRESULT NetworkPortMap(short Net, *Long inA, *Long inB,* Long outA,* Long outB,)

Interface

IFixturing6