Write-only |
Factory Preset Settings |
Description |
Application Object: Deletes all traces and windows. In addition, resets the analyzer to factory defined default settings and creates an S11 measurement named "CH1_S11_1" in window 1. Channel Object: Resets the channel (object) to factory defined default settings. Does NOT delete the current measurements or add a new measurement. |
VB Syntax |
app.Preset |
Variable |
(Type) - Description |
app |
An Application (object) |
chan |
A Channel (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.Preset |
C++ Syntax |
HRESULT Preset() |
Interface |
IApplication |