Preset the Analyzer


When you Preset the analyzer, it is set to known, or preset conditions. You can use the factory default preset conditions, or define your own User Preset conditions.

Note: Presetting the analyzer will not remove the calibration data in the Channel default CALREG calset.

See other 'Setup Measurements' topics

Preset Default Conditions

How to Preset the Analyzer

Using Hardkey/SoftTab/Softkey

  1. Press Preset > Main >  Preset.

When Confirm Preset is Off,

  1. Press Preset.

Tip: Press the Preset button to start the VNA application if it is not already running.

User Preset Conditions

The analyzer can be preset to either factory default conditions or User Preset conditions.

How to set User Preset

Using Hardkey/SoftTab/Softkey

  1. Press Preset > Main >  User Preset.

 

User Preset dialog box help

 

With a User Preset saved and enabled, when the VNA is Preset, the User Preset settings are recalled instead of the factory default settings. Calibration data is NOT recalled with a User Preset. Learn more about instrument state settings.

User Preset Enable
Check - The VNA is preset to User Preset conditions when the Preset button is pressed.
Clear - The VNA is preset to Default conditions when the Preset button is pressed.

Save current state as User Preset  Click to store the current instrument state as the User Preset conditions. File is stored as d

Load existing file as User Preset  Click to retrieve an instrument state to be used as the User Preset conditions.