Write-only |
Data Access Map |
Description |
Puts real and imaginary data into the specified location. This method forces the channel into Hold mode to prevent the input data from being overwritten. Learn more about reading and writing Cal Data using COM. Data put in the raw data store will be re-processed whenever a change is made to the measurement attributes such as format or correction. Data put in the measurement results store will be overwritten by any measurement attribute changes. See also putNAComplex |
VB Syntax |
measData.putComplex location, numPts, real(), imag(), [format] |
Variable |
(Type) - Description |
|
measData |
An IArrayTransfer interface which supports the Measurement object |
|
location |
(enum NADataStore) Where the Data will be put. Choose from: 0 - naRawData 1 - naCorrectedData 2 - naMeasResult 3 - naRawMemory 4 - naMemoryResult 5 - naDivisor - When reading data from, or writing data to, the normalization divisor, you must first create a divisor trace using DataToDivisor Method. |
|
numPts |
(long integer) - Number of data points in the channel |
|
real() |
(single) - Array containing real data values |
|
imag() |
(single) -Array containing imaginary data values |
|
format |
(enum NADataFormat) optional argument - display format of the real and imaginary data. Only used if destination is naMeasResult or naMemoryResult buffer. If unspecified, data is assumed to be in naDataFormat_Polar 0 - naDataFormat_LinMag 1 - naDataFormat_LogMag 2 - naDataFormat_Phase 3 - naDataFormat_Polar 4 - naDataFormat_Smith 5 - naDataFormat_Delay 6 - naDataFormat_Real 7 - naDataFormat_Imaginary 8 - naDataFormat_SWR 9 - naDataFormat_PhaseUnwrapped 10 - naDataFormat_InverseSmith 11 - naDataFormat_Kelvin 12 - naDataFormat_Fahrenheit 13 - naDataFormat_Centigrade |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Dim measData As IArrayTransfer |
C++ Syntax |
HRESULT putComplex( tagNADataStore DataStore, long lNumValues, float* pReal, float* pImag, tagDataFormat displayFormat) |
Interface |
IArrayTransfer |