Write-only
About Independent Power Calibration

Reset (Independent CalAll) Method


Description

This command resets all ranges for the given source port <n>.

 VB Syntax

IndependentPwrrCalPort.Reset

Variable

(Type) - Description

IndependentPwrrCalPort

A IndependentPowerCalibrationPort (object)

Return Type

Not Applicable

Default

Not Applicable

Example

CalibrateAllChannels.IndependentPowerCalibrationPort(3).Reset

C++ Syntax

HRESULT Reset

Interface

IIndependentPowerCalibrationPort