Write only
About ECal User Characterization

SaveToDiskMemory Method


Description

Saves the User Characterization to VNA disk memory. To save to ECal internal memory, use SaveToECal Method. User Characterization can be saved to both VNA disk memory and ECal module memory.

Note: An ECal confidence check can NOT be performed remotely from User Characterizations that are stored on the VNA disk.

 VB Syntax

userChar.SaveToDiskMemory (name)

Variable

(Type) - Description

userChar

An ECalUserCharacterizer (object)

name

(String) User characterization name. Although there is no limit to the number of characters, only about 10 characters appear in the Cal Wizard dialog when selecting a user characterization for use.

Return Type

Not Applicable

Default

Not Applicable

Examples

userChar.SaveToDiskMemory "DUT1"

C++ Syntax

HRESULT SaveToDiskMemory(BSTR name);

Interface

IECalUserCharacterizer2