Write-only
About PSAT Marker Search

SearchPowerSaturation Method


Description

Initiates a Power Saturation marker search.

Turns on and sets markers 1, 2, and 3 to calculate various Power Saturation parameters.

First set PMaxBackOff.

To turn off the Power Saturation markers, either turn them off individually or use DeleteAllMarkers Method

To search a User Range with the PSAT search, first activate marker 1 and set the desired User Range. Then send this command. The user range used with the PSAT search only applies to marker 1 searching for the linear gain value. The other markers may fall outside the user range.

 VB Syntax

pSat.SearchPowerSaturation( )

Variable

(Type) - Description

pSat

A PSaturation (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

pSat.SearchPowerSaturation

See example program

C++ Syntax

HRESULT SearchPowerSaturation()

Interface

IPSaturation