PSaturation Object


Description

Contains the methods and properties that initiate a Power Saturation marker search and returns PSAT data.

Accessing the PSaturation Object

Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application")

Dim PSat As PSaturation
Set PSat = app.ActiveMeasurement.PSaturation

See Also:

Methods

Interface

Description

SearchPowerSaturation

IPSaturation

Initiates a Power Saturation marker search.

Properties

 

Description

CompressionMax

IPSaturation

Returns the Compression Max result of a PSat marker search.

CompressionSaturation

IPSaturation

Returns the Compression Saturation result of a PSat marker search.

GainLinear

IPSaturation

Returns the Linear Gain result of a PSat marker search.

GainMax

IPSaturation

Returns the GainMax result of a PSAT marker search.

GainSaturation

IPSaturation

Returns the GainSaturation result of a PSAT marker search.

Pin

IPSaturation

Returns the Pin result of a PSAT marker search.

PMaxBackOff

IPSaturation

Sets and returns the backoff value used to calculate various PSAT parameters.

PMaxIn

IPSaturation

Returns the PMaxIn result of a PSAT marker search.

PMaxOut

IPSaturation

Returns the PMaxOut result of a PSAT marker search.

POut Property

IPSaturation

Returns the POut result of a PSAT marker search.

 

IPSaturation History

Interface

Introduced with VNA Rev:

IPSaturation

A.09.20