Write-only
About Mixer/Converter Settings

SegmentCalculate Method


Description

Calculates the specified parameter for the segment.

 VB Syntax

conv.SegmentCalculate index,param

Variable

(Type) - Description

conv

A Converter Object

index

(Long integer) Segment for which calculation is performed. Choose a segment between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer.

param

(Enum as ConverterCalculation)  Mixer port for which to calculate start and stop frequencies. Choose from:

 

enum

1st or only stage requires:

In addition, 2nd stage requires:

0

naCalculateINPUT

  • Output Start and Stop frequencies

  • LO frequency

  • Output sideband (High or Low)

  • IF Start and Stop frequencies

  • 2nd LO frequency

  • IF sideband (High or Low)

1

naCalculateINPUT AndOUTPUT

(2 stage mixers ONLY)

NA

  • IF Start and Stop frequencies

  • Both LO frequencies

2

naCalculateOUTPUT

  • Input Start and Stop frequencies

  • LO frequency

  • Output sideband (High or Low)

  • IF Start and Stop frequencies

  • 2nd LO frequency

  • IF sideband (High or Low)

3

naCalculateLO1

  • Input Start and Stop frequencies

  • Output frequency

  • Output sideband (High or Low)

  • IF Start and Stop frequencies

  • 2nd LO frequency

  • IF sideband (High or Low)

4

naCalculateLO2

NA

  • Input Start and stop frequencies

  • 1st LO start and stop frequencies

  • Output frequency

  • IF sideband(High or Low

  • Output sideband(High or Low)

Return Type

Not Applicable

Default

Not Applicable

Examples

mxr.SegmentCalculate 1,2 'Calculates the output frequencies for segment 1.

See example program

C++ Syntax

HRESULT SegmentCalculate(long index, ConverterCalculation param);

Interface

IConverter5