Write-only
 

UnselectCalSet Method


Description

Unselects a Cal Set from the channel.

 VB Syntax

channel.UnselectCalSet

Variable

(Type) - Description

channel

(object) - A Channel object

Return Type

Not Applicable

Default

Not Applicable

Example

channel.UnselectCalSet

C++ Syntax

HRESULT UnselectCalSet ();

Interface

IChannel24