Read-only
About the Handler IO Connector

get_Output Method


Description

Type 1 and Type2 configurations: Returns the last value written to the selected output pin.

Type3 configuration: Returns the current state of the selected output pin. If an Input1 trigger occurs, the state may not be the same value as was written.

All configurations: Data is written using put_Output Method.

 VB Syntax

data = handlerIo.get_Output (pin)

Variable

(Type) - Description

data

(variant) -  A variable to store the return value. The returned value will be one of the following:

0 - TTL Low

1 - TTL High

handlerIo

(object) - A HandlerIO object

pin

(enum as NAMatHandlerOutput) - output to read. Choose from:

naOutput1 (0)
naOutput1User (1)
naOutput2 (2)
naOutput2User (3)

Learn about User Output

Return Type

Variant

Default

Not Applicable

Examples

data = handlerIo.get_Output(naOutput1)

C++ Syntax

HRESULT get_Output ( tagNAMatHandlerOutput Output, VARIANT* Data );

Interface

IHWMaterialHandlerIO