Display Object

Description

Controls the settings of the front panel screen.

Accessing the Display object

Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)

Dim disp As IDisplay
Set disp = app.Display

See Also:

Method

Interface

See History

Description

None

 

 

Property

Interface

Description

PowerSpinResolution

IDisplay

Set and read the power level knob resolution.

IDisplay History

Interface

Introduced with PNA Rev:

IDisplay

13.25