Write/Read
About Power Level

PowerSpinResolution Property


Description

Sets and returns the resolution of the front panel knob when it is used to adjust Source Power manually.

 VB Syntax

disp.PowerSpinResolution = value

Variable

(Type) - Description

disp

A Display (object)

value

(Double) - Power level knob resolution. The range of acceptable values is 0.01 to 100.

Return Type

Double

Default

0.1

Examples

app.disp.PowerSpinResolution = 0.01 'Write - Every tick of the front panel knob will change the Power Level by 0.01 dBm.

resolution = app.disp.PowerSpinResolution 'Read - Get the current knob resolution.

C++ Syntax

HRESULT get_PowerSpinResolution(double* resolution)

HRESULT put_PowerSpinResolution(double resolution)

Interface

IDisplay