LimitSegment Object


Description

The LimitSegment object is an individual limit line.

Accessing the LimitSegment object

Get a handle to an individual limit line by using the LimitTest collection.

Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)

Dim limSegs As LimitTest
Set limSegs = app.ActiveMeasurement.LimitTest
limSegs(1).BeginResponse = 1000000000#

See Also:

Methods

Description

None

 

Properties

Description

BeginResponse

Specifies the Y-axis value that corresponds with Begin Stimulus (X-axis) value.

BeginStimulus

Specifies the beginning X-axis value of the Limit Line.

EndResponse

Specifies the Y-axis value that corresponds with End Stimulus (X-axis) value.

EndStimulus

Specifies the End X-axis value of the Limit Line.

Type

Specifies the Limit Line type.

 

LimitSegment History

Interface

Introduced with VNA Rev:

ILimitSegment

1.0