PortExtension Object  Superseded


ALL methods and properties on the PortExtension Object are Superseded with the Fixturing Object.

Description

Contains the methods and properties that control Port Extensions.

Accessing a PortExtension object

Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)

Dim PortExt As PortExtension
Set PortExt = app.PortExtension

See Also:

Methods

 

None

 

Property

Description

Input A

Sets the Input A extension value.

Input B

Sets the Input B extension value.

Input C

Sets the Input C extension value.

Port 1

Sets the Port 1 extension value.

Port 2

Sets the Port 2 extension value.

Port 3

Sets the Port 3 extension value.

State

Turns Port Extensions ON and OFF.

 

IPort Extension History

Interface

Introduced with VNA Rev:

IPort Extension

1.0