PowerSensors Collection


Description

A collection object that provides a mechanism for iterating through the PowerSensor objects which are connected to the power meter.  Each time this collection object is accessed, the power meter is queried to determine how many sensors are connected to it. The collection size and order of objects is then adjusted accordingly before the requested method or property operation is performed.  The power meter is specified by using the PowerMeterGPIBAddress property of the SourcePowerCalibrator object.

Accessing the PowerSensors Collection

Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)

Dim PwrSensors As PowerSensors
Set PwrSensors = app.SourcePowerCalibrator.PowerSensors

See Also:

 

Methods

Description

Item

Use to get a handle to a PowerSensor object in the collection.

Properties

Description

Count

Returns the number of objects in the collection.

Parent

Returns a handle to the Parent object (SourcePowerCalibrator) of this collection.