Read-only |
Description |
Returns a handle to the parent object of the collection object being referred to in the statement. The parent property allows the user to traverse from an object back up the object hierarchy. |
VB Syntax |
collection.Parent |
Variable |
(Type) - Description |
collection |
|
Return Type |
Object |
Default |
Not Applicable |
Examples |
parentobj = chans.Parent 'returns a handle to the parent object (Application) of the chans collection. -Read |
C++ Syntax |
HRESULT get_Parent(IApplication* *pApplication); //IChannels, IChannel, IMeasurements, INAWindows, and IExternalDevices HRESULT get_Parent(IChannel* *pChannel); //ITraces HRESULT get_Parent(INAWindow* *pWindow); //ISegments HRESULT get_Parent(IPowerSensor* *pSensor); //ICalFactorSegments(PMAR) HRESULT get_Parent(ISourcePowerCalibrator* *pCalibrator); //IPowerSensors, IPowerLossSegments, and IPowerMeterInterfaces |
Interface |
All listed above |