Write/Read |
About Pulse Measurements |
Description |
Choose to automatically or manually set pulse mode (Narrowband or Wideband) for the channel. |
VB Syntax |
pulseMeas.AutoDetection = bool |
Variable |
(Type) - Description |
|
pulseMeas |
A PulseMeasurementControl (object) |
|
bool |
False - Manually set the pulse mode. Use WideBandDectionState to set the pulse mode. True - Automatically set the pulse mode. |
Return Type |
Boolean |
Default |
True |
Examples |
pulse.AutoDetection = True 'Write |
|
value = pulse.AutoDetection 'Read |
|
C++ Syntax |
HRESULT get_AutoDetection(VARIANT_BOOL *pVal); HRESULT put_AutoDetection(VARIANT_BOOL newVal); |
Interface |
IPulseMeasurementControl |