Contains the properties for configuring pulse measurements in the PNA-X.
Some of these settings require Opt H08 / S93026A/B.
Learn about Integrated Pulse Application.
Dim app as AgilentPNA835x.Application
Dim chan as Channel
Set chan = app.ActiveChannel
Dim pulse as PulseMeasControl
Set pulse = chan.PulseMeasControl
The following shows how to make two new settings introduced with A.09.50:
|
Methods |
Description |
|
|---|---|---|
None |
|
|
Properties |
Interface |
Description |
IPulseMeasControl2 |
Sets the state of automatic CW sweep time in Pulse Profile mode. |
|
IPulseMeasControl |
Automatically or manually set pulse mode (Narrowband or Wideband) |
|
IPulseMeasControl |
Autoselect the IFBW |
|
AutoIFGain |
IPulseMeasControl |
For future use. |
IPulseMeasControl |
Auto-optimize pulse clock period |
|
IPulseMeasControl |
Autoselect Width and Delay |
|
IPulseMeasControl |
Autoselect Pulse Generators |
|
IPulseMeasControl2 |
Sets the pulse repetition frequency (PRF) for ALL internal pulse generators. |
|
IPulseMeasControl2 |
Sets the period for ALL internal pulse generators. |
|
IPulseMeasControl2 |
Sets the pulse width for ALL internal pulse generators. |
|
IPulseMeasControl |
Returns the channel object |
|
IPulseMeasControl |
Select Pulse Measurement selection |
|
IPulseMeasControl3 |
Sets and returns the start time of the profile pulse. |
|
IPulseMeasControl3 |
Sets and returns the stop time of the profile pulse. |
|
IPulseMeasControl2 |
This setting is used for troubleshooting purposes. |
|
IPulseMeasControl |
Select Narrowband or Wideband pulse detection. |
Interface |
Introduced with VNA Rev: |
IPulseMeasControl |
9.2 |
IPulseMeasControl2 |
9.40 |
IPulseMeasControl3 |
10.45 |