Write/Read
About Auto Port Extensions

AutoPortExtDCOffset Property


Description

Specifies whether or not to include DC Offset as part of automatic port extension. Learn more about Automatic DC Offset. Only allowed when  AutoPortExtLoss Property is set to ON.

 VB Syntax

fixture.AutoPortExtDCOffset = bool

Variable

(Type) - Description

fixture

A Fixturing (object)

bool

True - Includes DC Offset correction.

False - Does NOT include DC Offset correction.

Return Type

Boolean

Default

False

Examples

fixture.AutoPortExtDCOffset = True

value = fixture.AutoPortExtDCOffset 'Read

C++ Syntax

HRESULT get_AutoPortExtDCOffset(VARIANT_BOOL *pState);

HRESULT put_AutoPortExtDCOffset(VARIANT_BOOL bState);

Interface

IFixturing2