Write/Read
About Auto Port Extensions

AutoPortExtSearchStop Property


Description

Set the stop frequency for custom user span. Only applies when fixture.AutoPortExtConfig = 0 naAPEC_CSPN.

Learn more about User Span.

Only applies when fixture.AutoPortExtConfig = 0 naAPEC_CSPN

 VB Syntax

fixture.AutoPortExtSearchStop = value

Variable

(Type) - Description

fixture

A Fixturing (object)

value

(Double ) User span stop value. Must be within the frequency range of the active channel and greater than the value set by AutoPortExtSearchStart Property

Return Type

Double

Default

Stop frequency of the current active channel.

Examples

fixture.AutoPortExtSearchStop = 1E9

value = fixture.AutoPortExtSearchStop 'Read

C++ Syntax

HRESULT get_AutoPortExtSearchStop(double *pdVal );

HRESULT put_AutoPortExtSearchStop(double dVal);

Interface

IFixturing2