Write/Read |
About Averaging |
Description |
Specifies the number of measurements to combine for an average. Must also turn averaging ON by setting chan.Averaging = 1. |
VB Syntax |
chan.AveragingFactor = value |
Variable |
(Type) - Description |
chan |
A Channel (object) |
value |
(Long Integer) - Number of measurement sweeps to average. Choose any number between 1 and 65536 (2^16). |
Return Type |
Long Integer |
Default |
1 |
Examples |
chan.AveragingFactor = 5 'Write |
avgfact = chan.AveragingFactor ' Read |
|
C++ Syntax |
HRESULT get_AveragingFactor(long *pVal) |
Interface |
IChannel |