Write/Read
About Averaging

Averaging Property


Description

Turns trace averaging ON or OFF for all measurements on the channel. Averaging is only allowed on ratioed measurements; not on single input measurements.

 VB Syntax

chan.Averaging = state

Variable

(Type) - Description

chan

A Channel (object)

state

(boolean)
False
- Turns averaging OFF
True
- Turns averaging ON

Return Type

Boolean

Default

False

Examples

chan.Average = True 'Write

averg = chan.Averaging 'Read

C++ Syntax

HRESULT get_Averaging(BOOL *pVal)
HRESULT put_Averaging(BOOL newVal)

Interface

IChannel