| Write/Read | About Balanced Measurements | 
| Description | Sets and returns the measurement for the Balanced - Balanced topology. | ||||||||||||||||||||
| VB Syntax | balMeas.BBalMeasurement = value | ||||||||||||||||||||
| Variable | (Type) - Description | ||||||||||||||||||||
| balMeas | A BalancedMeasurement (object) | ||||||||||||||||||||
| value | (String) - Balanced - Balanced Measurement parameter. Not case sensitive. Choose from: 
 
 | ||||||||||||||||||||
| Return Type | String | ||||||||||||||||||||
| Default | Sdd11 | ||||||||||||||||||||
| Examples | balMeas.BBalMeasurement = "Sdd11" 'Write variable = balMeas.BBalMeasurement 'Read | ||||||||||||||||||||
| C++ Syntax | HRESULT get_BBalMeasurement(BSTR *pVal) HRESULT put_BBalMeasurement(BSTR newVal) | ||||||||||||||||||||
| Interface | IBalancedMeasurement | ||||||||||||||||||||