BalancedMeasurement Object


Description

These properties set the measurement type that is used with balanced topologies.

Use the BalancedTopology Object to set the topology and port mappings for the DUT,

Accessing the BalancedMeasurement object

Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)

Dim balMeas As BalancedMeasurement
Set balMeas = app.ActiveMeasurement.BalancedMeasurement

See Also:

 

(Bold Methods or Properties provide access to a child object)

Method

 

Description

None

 

 

Property

Interface

See History

Description

BalancedMode

IBalancedMeasurement

Sets and returns whether the balanced transform is ON or OFF.

BalancedStimulus

IBalancedMeasurement2

Sets and returns the stimulus properties of a balanced DUT.

BalancedTopology

IBalancedMeasurement

Sets and returns the topology of a balanced DUT.

BalSMeasurement

IBalancedMeasurement3

Sets and returns the measurement for the Balanced - Single-ended topology.

BBalMeasurement

IBalancedMeasurement

Sets and returns the measurement for the Balanced - Balanced topology.

BSSMeasurement

IBalancedMeasurement4

Sets and returns the measurement for the Balanced - Single-Ended - Single-Ended topology.

SBalMeasurement

IBalancedMeasurement

Sets and returns the measurement for the Single-Ended - Balanced topology.

SSBMeasurement

IBalancedMeasurement

Sets and returns the measurement for the Single-Ended - Single-Ended - Balanced topology

 

IBalancedMeasurement History

Interface

Introduced with VNA Rev:

IBalancedMeasurement

5.0

IBalancedMeasurement2

8.2

IBalancedMeasurement3

9.70

IBalancedMeasurement4

14.20