Write/Read
About Balanced Measurements

BSSMeasurement Property


Description

Sets and returns the measurement for the Balanced - Single-Ended - Single-Ended topology.

 VB Syntax

balMeas.BSSMeasurement = value

Variable

(Type) - Description

balMeas

A BalancedMeasurement (object)

value

(String) - Balanced - Single-Ended - Single-Ended Measurement parameter. Not case sensitive. Choose from:

 

Sdd11

Sdc11

Sds12

Sds13

Scd11

Scc11

Scs12

Scs13

Ssd21

Ssc21

Sss22

Sss23

Ssd31

Ssc31

Sss32

Sss33

Imbal1

Imbal2

Sds12/Scs12

Sds13/Scs13

 

Return Type

String

Default

Sdd11

Examples

balMeas.BSSMeasurement = "Sdd11" 'Write

variable = balMeas.BSSMeasurement  'Read

C++ Syntax

HRESULT get_BSSMeasurement(BSTR *pVal)

HRESULT put_BSSMeasurement(BSTR newVal)

Interface

IBalancedMeasurement4