Write/Read
About Marker Search

BandwidthTarget Property


Description

Sets the insertion loss value at which the bandwidth of a filter is measured (using BandwidthTracking or SearchFilterBandwidth). For example, if you want to determine the filter bandwidth 3 db below the bandpass peak value, set BandwidthTarget to -3.

 VB Syntax

meas.BandwidthTarget = value

Variable

(Type) - Description

meas

A Measurement (object)

value

(single) - Target value. Choose any number between -500 and 500

Return Type

Single

Default

-3

Examples

meas.BandwidthTarget = -3 'Write

fbw = meas.BandwidthTarget 'Read

C++ Syntax

HRESULT put_BandwidthTarget(float target)
HRESULT get_BandwidthTarget(float* target)

Interface

IMeasurement