Write/Read |
About Marker Search |
Description |
Searches continually (every sweep) for the current BandwidthTarget (default is -3). To search the filter bandwidth for ONE SWEEP only (not continually), use meas.SearchFilterBandwidth. This feature uses markers 1-4. To turn off these markers, either turn them off individually or DeleteAllMarkers. The bandwidth statistics are displayed on the analyzer screen. To get the bandwidth statistics, use either GetFilterStatistics or FilterBW, FilterCF , FilterLoss ,or FilterQ. The analyzer screen will show either Bandwidth statistics OR Trace statistics; not both. To restrict the search to a UserRange with the bandwidth search, first activate marker 1 and set the desired UserRange. Then send the SearchFilterBandwidth command. The user range used with bandwidth search only applies to marker 1 searching for the max value. The other markers may fall outside the user range. |
VB Syntax |
meas.BandwidthTracking = value |
Variable |
(Type) - Description |
meas |
A Measurement (object) |
value |
(boolean) |
Return Type |
Boolean |
Default |
False |
Examples |
meas.BandwidthTracking = False 'Write |
bwtrack = meas.BandwidthTracking 'Read |
|
C++ Syntax |
HRESULT put_BandwidthTracking(VARIANT_BOOL state) |
Interface |
IMeasurement |