Write/Read
About Modifying Cal Kits

CalKitType Property


Description

Sets and returns a calibration kit type to be used for UNGUIDED calibration and for cal kit modification. To get a handle to this kit, use app.ActiveCalKit.

Although an unlimited number of cal kits can be imported into the VNA, ONLY mechanical cal kits #1 through #95 can be accessed.

There is also a CalKitType property for use during a Guided, SMC, and VMC Calibration.

 VB Syntax

object.CalKitType = value

Variable

(Type) - Description

object

calkit (object) or

Application (object)

Note: app.CalKitType and calkit.calKitType perform exactly the same function.

value

(enum naCalKit) - Calibration Kit type. Choose from:

1 - naCalKit_User1
2 - naCalKit_User2
3 - naCalKit_User3
4 - naCalKit_User4
..
..
..

94 - naCalKit_User94
95 - naCalKit_User95

These enumerated values correspond with the calibration kit ID on the Advanced Cal Kit  Modify dialog box.

To change the cal kit name, use Name property.

Note: Always check the list of available cal kits using CalKitTypes to ensure that the correct cal kit is selected.

Return Type

NACalKit

Default

Not Applicable

Examples

calkit.CalKitType = naCalKit_User27

kitype = app.CalKitType

C++ Syntax

HRESULT get_CalKitType(tagNACalKit *pVal);
HRESULT put_CalKitType(tagNACalKit newVal);

Interface

IApplication
ICalKit