Write/Read
About Phase Reference Cal

CalSet Property


Description

Set and read the Cal Set name into which the calibration will be saved. The phase reference cal can NOT be saved to a cal register. The Cal Set is saved by calling GenerateErrorTerms at the conclusion of the Guided Cal.

 VB Syntax

phasRef.CalSet = value

Variable

(Type) - Description

phasRef

A PhaseReferenceCalibration Object

value

(String) Cal Set name.

Return Type

String

Default

Not Applicable

Examples

phase.CalSet = "PhaseRefCal"

See example program

C++ Syntax

HRESULT get_CalSet(BSTR CalSet* pVals);

HRESULT put_CalSet(BSTR CalSet newVals);

Interface

IPhaseReferenceCalibration