Write/Read
About Cal All

CalibrationPorts Property


Description

For each channel to be calibrated, sets and returns the ports to be calibrated. The port numbers need to be specified only for standard channels.  Apps channels have designated input/output/LO ports.  

Select any of the native VNA ports.

 VB Syntax

calAll.CalibrationPorts (chan) = ports

Variable

(Type) - Description

calAll

A CalibrateAllChannels (object)

chan

Channel to be calibrated with a Calibrate All Channels calibration.

port

(Variant Array) Ports to be calibrated for the specified channel.

Return Type

Variant Array

Default

Standard channels - ports 1 and 2

Apps channels - the designated input and output ports.

Examples

calAll.CalibrationPorts(2) = 0 'Ports to calibrate for channel 2

value = calAll.CalibrationPorts(2) 'returns the ports for channel 2

C++ Syntax

HRESULT get_CalibrationPorts (long channel, Variant ports);

HRESULT put_CalibrationPorts (long channel, Variant* ports);

Interface

ICalibrateAllChannels