Write/Read
About Cal All

Channels Property


Description

Sets and returns the list of channels to be calibrated during the Cal All session.

 VB Syntax

calAll.Channels  = chans

Variable

(Type) - Description

calAll

A CalibrateAllChannels (object)

chans

(Variant) Array of channel numbers to be calibrated, separated by commas. These channels must already exist.

Return Type

Variant

Default

The existing channels

Examples

calAll.Channels = Array(1,2,3) 'sets channels to be cal'd

chans = calAll.Channels 'returns the channel numbers to be cal'd

C++ Syntax

HRESULT get_Channels (VARIANT selectedChannels);

HRESULT put_Channels (VARIANT* selectedChannels);

Interface

ICalibrateAllChannels