Write/Read
About Gain Compression

CompressionInterpolation Property


Description

Sets whether or not interpolation should be performed on 2D measured compression data. Applies ONLY to 2D acquisition modes.

 VB Syntax

gca.CompressionInterpolation = value

Variable

(Type) - Description

gca

A GainCompression (object)

value

(boolean) - Choose from:

True  Interpolate the results

False  Do NOT interpolate the results but return the value closest to compression.

Return Type

Boolean

Default

False

Examples

gca.CompressionInterpolation = True 'Write

compInt = gca.CompressionInterpolation 'Read

C++ Syntax

HRESULT get_CompressionInterpolation(VARIANT_BOOL* pVal)

HRESULT put_CompressionInterpolation(VARIANT_BOOL newVal)

Interface

IGainCompression