Read-only
About PNOP / PSAT Marker Search

CompressionMax Property


Description

Returns the Compression Max result of a PSat or PNOP marker search.

Comp Max =  Gain Max - Linear Gain (not shown on PNOP marker readout).

 VB Syntax

compMax = pMarker.CompressionMax

Variable

(Type) - Description

compMax

(double) - Variable to store returned value

pMarker

A PNOP (object) or a PSaturation (object)

Return Type

Double

Default

Not applicable

Examples

compMax = pMark.CompressionMax 'Read

See example program

C++ Syntax

HRESULT get_CompressionMax(double* pNewVal)

Interface

IPNOP or IPSaturation